AXIS#.CS.STATE
Description
AXIS#.CS.STATE returns the internal state machine value of the controlled stop.
0 = controlled stop is not occurring.
1 = controlled stop is occurring
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.CS.STATE | 0x5002 | 0x1 | USINT | - | - | RO | False |
AXIS2.CS.STATE | 0x5102 | 0x1 | USINT | - | - | RO | False |